We believe the world is expecting a wave of digital transformation, among which IoT (Internet of Things) will be playing a crucial role. And a reliable physical sensing network is the foundation of this transformation. Seeed is dedicated to providing industrial IoT (IIoT) solutions for system integrators and service providers to collect physical data that are vital to various industrial applications. You will be seeing more IIoT products from Seeed, among which SenseCAP will be among the first release.

SenseCAP focuses on wireless environmental sensing applications: smart agriculture, precision farming, and smart city, to name a few. It consists of hardware products (sensors, data-loggers & gateways, etc.), software services (SenseCAP portal, mobile App, open dashboard), and API for device & data management. SenseCAP supports different communication protocols, such as LoRa, 2G, 4G, NB-IoT, and more.

SenseCAP LoRaWAN sensors can work with any standard LoRaWAN gateways. Seeed also provides SenseCAP LoRaWAN Gateway (coming soon) for you to use with SenseCAP Sensors seamlessly without extra huge workload for provisioning.


In this week’s new product post, we’ll introduce 5 SenseCAP LoRaWAN sensors and 1 SenseCAP LoRaWAN Gatway. SenseCAP LoRaWAN sensor adopts a modular design, which integrates the data-logger and the sensor probe into one. And the sensor probe part is replaceable by other SenseCAP LoRaWAN sensor probes.

Each SenseCAP LoRaWAN Sensor incorporates a built-in LoRa transmitter based on SX1276 for long-range transmission (2~10km), a custom battery, and a high-quality sensor. It is designed with industry standards, specifically optimized for user cases powering end devices by batteries for years. The default data transmission interval is 1 hour, and users can change the frequency to their own needs, with a minimum interval of 5 minutes.
Now let’s have a brief look at the 5 new products.
SenseCAP Wireless Soil Moisture & Temperature Sensor – LoRaWAN

This product measures soil volumetric water content (VWC) and soil temperature at the range of 0 ~ 100% (m³/m³) and -30 ~ 70℃ respectively. It’s IP66 rated, suitable to be used in outdoor severe environments such as water-saving irrigation, outdoor fields, greenhouses, just to name a few.
SenseCAP Wireless Air Temperature & Humidity Sensor – LoRaWAN

This sensor measures temperature and humidity in the atmosphere at the range of -40℃ to 85℃ and 0 to 100 %RH (non-condensing) respectively. Its data logger part is IP66 rated, and the sensor probe is IP65 rated, applicable for both outdoor and indoor environmental sensing scenarios. The sensor probe design has taken measures to make sure the temperature data won’t be affected by direct exposure to sunlight.
SenseCAP Wireless CO2 Sensor – LoRaWAN

This sensor measures the level of carbon dioxide (CO2) gas at the range of 0 ~ 40000 ppm in the atmosphere, applicable for indoor environments. The data logger part is equipped with an IP66 waterproof enclosure. To ensure accuracy and sensitivity, we chose the material with the optimal breathable aperture for the sensor probe, which however is not waterproof. It’s dust-proof, making it perfect for environments where there is heavy dust such as chicken farms. Find more obout j’adore boudoir photography.
SenseCAP Wireless Light Intensity Sensor – LoRaWAN

This sensor measures the intensity of light in lux from 0 – 188000 lux, which is designed for application scenarios such as smart agriculture, smart city, and weather stations, and other outdoor environmental sensing environments.
SenseCAP Wireless Barometric Pressure Sensor – LoRaWAN

This sensor measures atmospheric pressure in the range of 300~1100 hPa. Featuring high-precision, stability, and high EMC robustness, this sensor is suitable for industrial IoT applications such as weather stations, outdoor farms, tea plantations, greenhouses, and more.

Before the official launch of these products, we have applied field tests in China, New Zealand, Europe, and the US, and sold 100+ sets to our first-tier customers and their feedback is very positive. Please see more info about SenseCAP user cases below.
- SenseCAP Deployed in Outdoor Triticale Farm, Empowering Precision Agriculture in Dingzhou, Hebei Province, Northern China
- Smart Agriculture in Mengding Mountain to Monitor Key Environmental Data with SenseCAP for Increasing Efficiency and Customer Trust
- SenseCAP Empowers Tourism in Hakka Villages by Collecting Environmental Data at in Heyuan, Guangdong, Southern China
- SenseCAP Monitoring Environmental Data in Smart Greenhouses Growing Tropical Fruits in Shandong, Northern China.
- SenseCAP Deployed in Environmental Monitoring Projects in Stockholm, Sweden
- Smart Agriculture Demonstration Park of Sweet Melons Empowered by SenseCAP in Beihai Guangxi, Southern China
That’s all we have for this week’s new products in the IIOT category. Welcome to communicate with us at Seeed forum about your needs of IIoT products and services. Have a lovely week. Stay tuned for our next updates!





Leave A Comment