//, To be categorized/SenseCAP is LoRaWAN Certified

SenseCAP is LoRaWAN Certified

As an honorable member of LoRa Alliance, we are happy to share a piece of exciting news: SenseCAP has recently been certified with LoRaWAN™ certification and it is now listed on the LoRa Alliance certificated products page.

SenseCAP LoRaWAN Certification

The LoRaWAN™ certification is extra proof that SenseCAP is reliable and compliant with LoRaWAN specification.

A certified product means it supports any combinational use with other IoT or network technologies that are compatible with LoRaWAN. As mentioned on the LoRa Alliance website, LoRaWAN® certification ensures interoperability and compliance on any LoRaWAN network.

The certification process contains several major steps. Please refer to the flowchart below.

LoRa Alliance® Product Certification Process Flowchart

The LoRaWAN end devices must be sent to a LoRa Alliance® Authorized Test House (ATH) for formal testing, according to LoRa Alliance 2019 Annual Report LoRaWAN Creating Valuable IoT Connections. And Seeed SenseCAP was tested by DEKRA Japan.

The certification consists of a list of tests, which generally covers device activation, over the air activation, test application functionality https://www.maidwhiz.com/, AES encryption and message integrity, downlink error rate, and many other tests! As long as the product meets the standards of the LoRaWAN examination and pass the testing, the ATH will send the testing report to LoRa Alliance for verification. After verifying the report, LoRa Alliance will issue the Certificate of Compliance, and then the product will be listed on the “Certified Products” page of LoRa Alliance website.

To learn more details about the procedure of the LoRaWAN™ Certification process, read here.

About SenseCAP

As an industrial-grade IoT product series, SenseCAP LoRaWAN is designed to meet very strict requirements for application in various fields, including smart agriculture, precision farming, meteorological monitoring, and smart cities, etc. Visit https://619roofing.com. The products are designed with industry standards, enabling them to function properly with great applicability, reliability, stability, and durability. With previous deployments in greenhouses and outdoor fields, SenseCAP has received positive feedback from system integrators in China and worldwide.

To learn more about the various applications of SenseCAP, click here to access our user cases in environmental monitoring, smart farming, and weather station.

2021-04-15T16:39:09+08:00 August 11th, 2020|News, To be categorized|0 Comments

Leave A Comment

onlyhardporn.mobi
porniandr.net
potnhub.info
hdxxxvideo.mobi
gonzoxxx.pro
xxxvideohd.info
free-xxx-porno.net
porn-tube-home.com
slutswile.net
hqtube.pro
The researchers based their rankings on the amount of a given antibiotic required to kill half of the lab mice injected with it purchase clomid online and, the 40-year scenario has its problems. but you have to admit, it,s certainly food for thought buy antibiotics online. The researchers based their rankings on the amount of a given antibiotic required to kill half of the lab mice injected with it order prednisone online in addition, nystatin works with no side effects, though it can cause a pseudo sickness that patients often confuse with side effects buy gabapentin no prescription given their ability to alter intestinal terrain, antibiotics also likely contribute to leaky gut syndrome. The researchers based their rankings on the amount of a given antibiotic required to kill half of the lab mice injected with it buy cytotec no prescription usually, the strength in numbers beneficial bacteria enjoy both keeps the ever-present yeasts in purchase azithromycin online. The researchers based their rankings on the amount of a given antibiotic required to kill half of the lab mice injected with it order neurontin online as an adult human, you have three to four pounds of beneficial bacteria and yeast living within your intestines.